AXIS#.MOTOR.PHASE
Description
This parameter is the relative alignment of the feedback to the motor coils. For Kollmorgen motors, the feedback and coils are aligned, and AXIS#.MOTOR.PHASE may be set to 0.
-
-
If MOTOR.AUTOSET = 1 and motor memory version is 0.2 or greater, this parameter is automatically configured for Kollmorgen motors.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Electrical degrees |
|
Range |
0 to 360 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.PHASE | 0x500B | 0x15 | UINT | - | - | RW | False |
| AXIS2.MOTOR.PHASE | 0x510B | 0x15 | UINT | - | - | RW | False |